Acsis™

ACSIS™ (Automated Composite Structure Inspection System) is Ingersoll Machine Tools’ best-in-class solution for the automated inspection, repair, and quality monitoring of the composite manufacturing process.

Acsis

First released in 2016, ACSIS™has become the industry-leader in automated inspection with unparalleled abilities to locate, identify, and measure layup defects such as overlaps, gaps, twists, missing tows, splices, and more, on a variety of materials.

Defects Detection

All identified defects are presented to the operator for review and input via an interactive tablet/smart-watch application paired with a laser projector or an Augmented Reality interface using the Microsoft HoloLens.

perator feedback during this process is used to further refine ACSIS™‘s machine learning models which are then requalified via Ingersoll’s patented training software. Beyond defect detection, all results are also electronically logged for further review offline in the Defect Cloud interface to identify trends in defect occurrences and improve the production of future parts or current parts by offering insight to machine health.

ACSIS™ has shown a defect detection rate of over 99% and has been qualified in production to existing NDI standards.

Configuration:

  • “In-ply" configuration to accomodate the in-situ inspection of large structures
  • ”Post-ply” automatically exchangeable module where complex geometry demands it
Business continuity of Camozzi Group Companies during Covid-19 outbreak

We inform that the production lines of Camozzi Group Companies are running and all the services and assistance are guaranteed to our customers worldwide.

With reference to the restrictions decided by the Official Authorities in Italy for the containment of the Covid-19 outbreak - especially the Prime Minister’s Decree of March 8,2020 - we confirm the decree  does not affect our business processes even included transportation of goods.

Camozzi Group has implemented all special prevention and control measures in compliance with the principles and the guidelines provided by the World Health Organization and the Italian Ministry of Health in coordination with the Italian Ministries.

Continuità operativa delle aziende del Gruppo Camozzi durante la contingenza Covid-19

Informiamo che la produzione delle aziende appartenenti al Gruppo Camozzi sta funzionando regolarmente e tutti i servizi ed assistenza sono garantiti ai nostri clienti a livello internazionale.

In relazione alle restrizioni decise dalle Autorità Governative Italiane per il contenimento della diffusione del Covid-19, con specifico riferimento al Decreto del Primo Ministro dell’ 8 Marzo 2020, confermiamo che al momento tale Decreto non incide sulle nostre attività e processi, incluso il trasporto delle merci.

Il Gruppo Camozzi ha implementato tutte le misure speciali di controllo e prevenzione in conformità ai principi e linee guida forniti dall’Organizzazione Mondiale della Sanità, dal Ministero della Salute Italiano in coordinamento con tutti i  Ministeri Italiani.