Fiber placement machines

The Division offers the Ingersoll range of automated fiber placement machines for the manufacturing of complex and ultra-high performance composite parts, such as aircraft wings

Mongoose™ is Ingersoll Machine Tools’ iconic Fiber Placement Machine first introduced in 2009. Since then Mongoose™ has become the aerospace industry preferred solution for the carbon fiber layup of tight concave parts and complex geometry convex tools. Its recent evolution, Mongoose Hybrid, features AFP (Automated Fiber Placement), ATL (Automated Tape Layer), trimming and inspection on the same machine platform to cover any need of composite manufacturing.

The Mongoose series includes a variety of configurations, including gantry and robotic, each suited to different part geometries and that can be used with a wide variety of resins and fibers. As such Mongoose’s flexibility can provide a solution to almost any application requirement.

Moongoose™

Mongoose™ is Ingersoll iconic Fiber Placement Machine first released in 2009.

Mongoose Hybrid™

Mongoose Hybrid™ is the latest evolution of Ingersoll Machine Tools iconic AFPM first released in 2009.

Robotic FP™

Robotic FP™ is Ingersoll Machine Tools’ robotic solution for mid-size, complex geometry, composite layup.

Hawk™

Hawk™ is Ingersoll Machine Tools’ new Fiber Placement Module engineered for high productivity and high reliability layups of large aerostructure parts: wings, fuselages, fairings…

Acsis™

ACSIS™ (Automated Composite Structure Inspection System) is Ingersoll Machine Tools’ best-in-class solution for the automated inspection, repair, and quality monitoring of the composite manufacturing process.

Business continuity of Camozzi Group Companies during Covid-19 outbreak

We inform that the production lines of Camozzi Group Companies are running and all the services and assistance are guaranteed to our customers worldwide.

With reference to the restrictions decided by the Official Authorities in Italy for the containment of the Covid-19 outbreak - especially the Prime Minister’s Decree of March 8,2020 - we confirm the decree  does not affect our business processes even included transportation of goods.

Camozzi Group has implemented all special prevention and control measures in compliance with the principles and the guidelines provided by the World Health Organization and the Italian Ministry of Health in coordination with the Italian Ministries.

Continuità operativa delle aziende del Gruppo Camozzi durante la contingenza Covid-19

Informiamo che la produzione delle aziende appartenenti al Gruppo Camozzi sta funzionando regolarmente e tutti i servizi ed assistenza sono garantiti ai nostri clienti a livello internazionale.

In relazione alle restrizioni decise dalle Autorità Governative Italiane per il contenimento della diffusione del Covid-19, con specifico riferimento al Decreto del Primo Ministro dell’ 8 Marzo 2020, confermiamo che al momento tale Decreto non incide sulle nostre attività e processi, incluso il trasporto delle merci.

Il Gruppo Camozzi ha implementato tutte le misure speciali di controllo e prevenzione in conformità ai principi e linee guida forniti dall’Organizzazione Mondiale della Sanità, dal Ministero della Salute Italiano in coordinamento con tutti i  Ministeri Italiani.